CompanionResultBuilderCompanionResultDisposition Enumeration¶
NXOpen.CAE.CompanionResultBuilder.CompanionResultDisposition is an alias for NXOpen.CAE.CompanionResultBuilderCompanionResultDisposition
-
class
NXOpen.CAE.
CompanionResultBuilderCompanionResultDisposition
¶ Bases:
object
Companion result disposition indicates how the Companion result will be disposed of when primary result is deleted.
Enum Members
Enum Member Enum Member Description Delete Companion Result Object will be deleted when primary results are deletedKeep The Companion Result Object will be keep when primary results are deleted so that when the primary results are later regenerated these companion results will again be available.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-