FlatPatternsBuilder Class¶
-
class
NXOpen.CAE.
FlatPatternsBuilder
¶ Bases:
NXOpen.Builder
Represents a Flat Patterns Builder.
To create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateFlatPatternsBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Filename | Returns or sets the string0 |
IndividualExport | Returns or sets the individual export |
PlySelect | Returns or sets the ply select |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExportButton | TODO: fill in a description for this |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Filename¶
-
FlatPatternsBuilder.
Filename
¶ Returns or sets the string0
-------------------------------------
Getter Method
Signature
Filename()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Filename(filename)
Parameters: filename (str) – New in version NX6.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
IndividualExport¶
-
FlatPatternsBuilder.
IndividualExport
¶ Returns or sets the individual export
-------------------------------------
Getter Method
Signature
IndividualExport()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndividualExport(individualExport)
Parameters: individualExport (bool) – New in version NX6.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
PlySelect¶
-
FlatPatternsBuilder.
PlySelect
¶ Returns or sets the ply select
-------------------------------------
Getter Method
Signature
PlySelect()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlySelect(plySelect)
Parameters: plySelect (int) – New in version NX6.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Method Detail¶
ExportButton¶
-
FlatPatternsBuilder.
ExportButton
¶ TODO: fill in a description for this
Signature
ExportButton()
New in version NX6.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
Validate¶
-
FlatPatternsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.