PostGraphBuilderDataErrorHandling Enumeration¶
NXOpen.CAE.PostGraphBuilder.DataErrorHandling is an alias for NXOpen.CAE.PostGraphBuilderDataErrorHandling
-
class
NXOpen.CAE.
PostGraphBuilderDataErrorHandling
¶ Bases:
object
error handling option when result values are not present for the selected entities
Enum Members
Enum Member Enum Member Description Skip UserValue User given value will used for those entities which do not have result value associated with them-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-