ElementTranslateBuilder Class¶
-
class
NXOpen.CAE.
ElementTranslateBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementTranslateBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementTranslateBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the coordinate system to be used for translating the selected elements |
Distance | Returns the total distance for translation along a vector |
DistanceOption | Returns or sets the distance option |
ElementDimension | Returns or sets the dimension of the elements to be translated |
ElementSelection | Returns the selected elements |
ElementType | Returns the element type builder. |
ExportMesh | Returns or sets the option which indicates whether mesh is exported to solver or not. |
FlipState | Returns or sets the flip state from the builder |
Increment | Returns or sets the increment in label for each new element |
Label | Returns or sets the start label for the new elements |
LabelOption | Returns or sets the option to specify the start label and increment for the new elements OR specify an offset from the existing element labels |
MeshCollectorName | Returns or sets the name of the mesh collector which will hold the new elements |
MeshName | Returns or sets the name of the mesh that will hold the new elements |
Method | Returns or sets the method to be used for translating the selected elements |
NeutralName | Returns or sets the neutral name of the elements to be created |
NewMeshOption | Returns or sets the option to create a new mesh or add the new elements to an existing mesh |
NumCopy | Returns or sets the number of copies to be created for each selected element |
Offset | Returns or sets the offset to be used to generate new element labels |
PAngle | Returns the phi angle for translation in a spherical coordinate system |
RDistance | Returns the radial component of distance for translation in a cylindrical/spherical coordinate system |
TAngle | Returns the theta angle for translation in a cylindrical/spherical coordinate system |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the vector along which the selected elements should be translated |
XDistance | Returns the x component of distance for translation in a cartesian coordinate system |
YDistance | Returns the y component of distance for translation in a cartesian coordinate system |
ZDistance | Returns the z component of distance for translation in a cartesian/cylindrical coordinate system |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementTranslateBuilderDistanceType Enumeration | Distance - specify whether the translation distance is per copy or total |
ElementTranslateBuilderElemDimensionType Enumeration | Dimension of the elements to be created |
ElementTranslateBuilderLabelType Enumeration | Option to use label/increment or offset |
ElementTranslateBuilderMethodType Enumeration | Translation method |
ElementTranslateBuilderNewMeshType Enumeration | Option to create a new mesh or add the new elements to an existing mesh |
Property Detail¶
Csys¶
-
ElementTranslateBuilder.
Csys
¶ Returns or sets the coordinate system to be used for translating the selected elements
-------------------------------------
Getter Method
Signature
Csys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys(csys)
Parameters: csys ( NXOpen.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Distance¶
-
ElementTranslateBuilder.
Distance
¶ Returns the total distance for translation along a vector
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DistanceOption¶
-
ElementTranslateBuilder.
DistanceOption
¶ Returns or sets the distance option
-------------------------------------
Getter Method
Signature
DistanceOption()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilderDistanceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceOption(distanceOption)
Parameters: distanceOption ( NXOpen.CAE.ElementTranslateBuilderDistanceType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementDimension¶
-
ElementTranslateBuilder.
ElementDimension
¶ Returns or sets the dimension of the elements to be translated
-------------------------------------
Getter Method
Signature
ElementDimension()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilderElemDimensionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementDimension(elementDimension)
Parameters: elementDimension ( NXOpen.CAE.ElementTranslateBuilderElemDimensionType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementSelection¶
-
ElementTranslateBuilder.
ElementSelection
¶ Returns the selected elements
-------------------------------------
Getter Method
Signature
ElementSelection()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX5.0.0.
License requirements: None.
ElementType¶
-
ElementTranslateBuilder.
ElementType
¶ Returns the element type builder.
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ExportMesh¶
-
ElementTranslateBuilder.
ExportMesh
¶ Returns or sets the option which indicates whether mesh is exported to solver or not.
-------------------------------------
Getter Method
Signature
ExportMesh()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExportMesh(fExportMesh)
Parameters: fExportMesh (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FlipState¶
-
ElementTranslateBuilder.
FlipState
¶ Returns or sets the flip state from the builder
-------------------------------------
Getter Method
Signature
FlipState()
Returns: Return type: int New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
FlipState(flipstate)
Parameters: flipstate (int) – New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Increment¶
-
ElementTranslateBuilder.
Increment
¶ Returns or sets the increment in label for each new element
-------------------------------------
Getter Method
Signature
Increment()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment(increment)
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
ElementTranslateBuilder.
Label
¶ Returns or sets the start label for the new elements
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label(label)
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
LabelOption¶
-
ElementTranslateBuilder.
LabelOption
¶ Returns or sets the option to specify the start label and increment for the new elements OR specify an offset from the existing element labels
-------------------------------------
Getter Method
Signature
LabelOption()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilderLabelType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelOption(labelOption)
Parameters: labelOption ( NXOpen.CAE.ElementTranslateBuilderLabelType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshCollectorName¶
-
ElementTranslateBuilder.
MeshCollectorName
¶ Returns or sets the name of the mesh collector which will hold the new elements
-------------------------------------
Getter Method
Signature
MeshCollectorName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshCollectorName(meshCollectorName)
Parameters: meshCollectorName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshName¶
-
ElementTranslateBuilder.
MeshName
¶ Returns or sets the name of the mesh that will hold the new elements
-------------------------------------
Getter Method
Signature
MeshName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshName(meshName)
Parameters: meshName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method¶
-
ElementTranslateBuilder.
Method
¶ Returns or sets the method to be used for translating the selected elements
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilderMethodType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Method(method)
Parameters: method ( NXOpen.CAE.ElementTranslateBuilderMethodType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NeutralName¶
-
ElementTranslateBuilder.
NeutralName
¶ Returns or sets the neutral name of the elements to be created
-------------------------------------
Getter Method
Signature
NeutralName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeutralName(neutralName)
Parameters: neutralName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewMeshOption¶
-
ElementTranslateBuilder.
NewMeshOption
¶ Returns or sets the option to create a new mesh or add the new elements to an existing mesh
-------------------------------------
Getter Method
Signature
NewMeshOption()
Returns: Return type: NXOpen.CAE.ElementTranslateBuilderNewMeshType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewMeshOption(newMeshOption)
Parameters: newMeshOption ( NXOpen.CAE.ElementTranslateBuilderNewMeshType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumCopy¶
-
ElementTranslateBuilder.
NumCopy
¶ Returns or sets the number of copies to be created for each selected element
-------------------------------------
Getter Method
Signature
NumCopy()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumCopy(numCopy)
Parameters: numCopy (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Offset¶
-
ElementTranslateBuilder.
Offset
¶ Returns or sets the offset to be used to generate new element labels
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PAngle¶
-
ElementTranslateBuilder.
PAngle
¶ Returns the phi angle for translation in a spherical coordinate system
-------------------------------------
Getter Method
Signature
PAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
RDistance¶
-
ElementTranslateBuilder.
RDistance
¶ Returns the radial component of distance for translation in a cylindrical/spherical coordinate system
-------------------------------------
Getter Method
Signature
RDistance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
TAngle¶
-
ElementTranslateBuilder.
TAngle
¶ Returns the theta angle for translation in a cylindrical/spherical coordinate system
-------------------------------------
Getter Method
Signature
TAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Vector¶
-
ElementTranslateBuilder.
Vector
¶ Returns or sets the vector along which the selected elements should be translated
-------------------------------------
Getter Method
Signature
Vector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
XDistance¶
-
ElementTranslateBuilder.
XDistance
¶ Returns the x component of distance for translation in a cartesian coordinate system
-------------------------------------
Getter Method
Signature
XDistance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
YDistance¶
-
ElementTranslateBuilder.
YDistance
¶ Returns the y component of distance for translation in a cartesian coordinate system
-------------------------------------
Getter Method
Signature
YDistance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ZDistance¶
-
ElementTranslateBuilder.
ZDistance
¶ Returns the z component of distance for translation in a cartesian/cylindrical coordinate system
-------------------------------------
Getter Method
Signature
ZDistance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ElementTranslateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.