LaminateSpreadsheetReportBuilderEnvelopeRule Enumeration¶
NXOpen.CAE.LaminateSpreadsheetReportBuilder.EnvelopeRule is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderEnvelopeRule
-
class
NXOpen.CAE.
LaminateSpreadsheetReportBuilderEnvelopeRule
¶ Bases:
object
Result enveloping rules.
When there is more than one solutions or loadcases, defines which result to keep and display in the graphical report
Enum Members
Enum Member Enum Member Description MaxMin Keep minimum and maximum valuesMin Keep minimum valuesMax Keep maximum valuesAbsMax Keep maximum absolute valuesAbsMin Keep minimum absolute values-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-