DurabilityResultsReportBuilder Class¶
-
class
NXOpen.CAE.
DurabilityResultsReportBuilder
¶ Bases:
NXOpen.Builder
Represents the builder for reporting the durability results.
To create a new instance of this class, use
NXOpen.CAE.DurabilityManager.CreateDurabilityResultsReportBuilder
Default values.
Property Value EventDamage 1 EventLife 0 FailureIndex 0 FatigueSafetyFactor 0 MarginSafety 0 StrengthSafetyFactor 0 UseEvents Active UseHighlight 0 New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
EventDamage | Returns or sets the event damage toggle |
EventLife | Returns or sets the event life toggle |
FailureIndex | Returns or sets the failure index toggle |
FatigueSafetyFactor | Returns or sets the fatigue safety factor toggle |
FreeFaceIndicator | Returns or sets the free face indicator. |
LoadProportionality | Returns or sets the load proportionality. |
MarginSafety | Returns or sets the margin safety toggle |
PrincipalAxisStability | Returns or sets the principal axis stability. |
StrengthSafetyFactor | Returns or sets the strength safety factor toggle |
Tag | Returns the Tag for this object. |
UseEvents | Returns or sets the use events pop-up menu |
UseHighlight | Returns or sets the use highlight toggle |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExportResultsToCsv | Export durability results to a csv file. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityResultsReportBuilderUseEventsEnum Enumeration | the event report options enum. |
Property Detail¶
EventDamage¶
-
DurabilityResultsReportBuilder.
EventDamage
¶ Returns or sets the event damage toggle
-------------------------------------
Getter Method
Signature
EventDamage()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventDamage(eventDamage)
Parameters: eventDamage (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EventLife¶
-
DurabilityResultsReportBuilder.
EventLife
¶ Returns or sets the event life toggle
-------------------------------------
Getter Method
Signature
EventLife()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventLife(eventLife)
Parameters: eventLife (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FailureIndex¶
-
DurabilityResultsReportBuilder.
FailureIndex
¶ Returns or sets the failure index toggle
-------------------------------------
Getter Method
Signature
FailureIndex()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FailureIndex(failureIndex)
Parameters: failureIndex (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueSafetyFactor¶
-
DurabilityResultsReportBuilder.
FatigueSafetyFactor
¶ Returns or sets the fatigue safety factor toggle
-------------------------------------
Getter Method
Signature
FatigueSafetyFactor()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueSafetyFactor(fatigueSafetyFactor)
Parameters: fatigueSafetyFactor (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FreeFaceIndicator¶
-
DurabilityResultsReportBuilder.
FreeFaceIndicator
¶ Returns or sets the free face indicator.
-------------------------------------
Getter Method
Signature
FreeFaceIndicator()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FreeFaceIndicator(freeFaceIndicator)
Parameters: freeFaceIndicator (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
LoadProportionality¶
-
DurabilityResultsReportBuilder.
LoadProportionality
¶ Returns or sets the load proportionality.
-------------------------------------
Getter Method
Signature
LoadProportionality()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadProportionality(loadProportionality)
Parameters: loadProportionality (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MarginSafety¶
-
DurabilityResultsReportBuilder.
MarginSafety
¶ Returns or sets the margin safety toggle
-------------------------------------
Getter Method
Signature
MarginSafety()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MarginSafety(marginSafety)
Parameters: marginSafety (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PrincipalAxisStability¶
-
DurabilityResultsReportBuilder.
PrincipalAxisStability
¶ Returns or sets the principal axis stability.
-------------------------------------
Getter Method
Signature
PrincipalAxisStability()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalAxisStability(principalAxisStability)
Parameters: principalAxisStability (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
StrengthSafetyFactor¶
-
DurabilityResultsReportBuilder.
StrengthSafetyFactor
¶ Returns or sets the strength safety factor toggle
-------------------------------------
Getter Method
Signature
StrengthSafetyFactor()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StrengthSafetyFactor(strengthSafetyFactor)
Parameters: strengthSafetyFactor (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
UseEvents¶
-
DurabilityResultsReportBuilder.
UseEvents
¶ Returns or sets the use events pop-up menu
-------------------------------------
Getter Method
Signature
UseEvents()
Returns: Return type: NXOpen.CAE.DurabilityResultsReportBuilderUseEventsEnum
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseEvents(useEvents)
Parameters: useEvents ( NXOpen.CAE.DurabilityResultsReportBuilderUseEventsEnum
) –New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
UseHighlight¶
-
DurabilityResultsReportBuilder.
UseHighlight
¶ Returns or sets the use highlight toggle
-------------------------------------
Getter Method
Signature
UseHighlight()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseHighlight(useHighlight)
Parameters: useHighlight (bool) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
ExportResultsToCsv¶
-
DurabilityResultsReportBuilder.
ExportResultsToCsv
¶ Export durability results to a csv file.
Signature
ExportResultsToCsv(csvFilename)
Parameters: csvFilename (str) – durability report will be written-out to this file. NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Validate¶
-
DurabilityResultsReportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.