LbcAssociationMgr Class¶
-
class
NXOpen.CAE.
LbcAssociationMgr
¶ Bases:
NXOpen.Builder
Represents an abstract
NXOpen.CAE.LbcAssociationMgr
This is an abstract class
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TypeOption | Returns or sets the bc type option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExportToCsv | Export to csv |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ImportFromCsv | Import from csv |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LbcAssociationMgrBcType Enumeration | Option to associate bc type, load, constraint or simulation objects |
Property Detail¶
TypeOption¶
-
LbcAssociationMgr.
TypeOption
¶ Returns or sets the bc type option
-------------------------------------
Getter Method
Signature
TypeOption()
Returns: Return type: NXOpen.CAE.LbcAssociationMgrBcType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TypeOption(entityOption)
Parameters: entityOption ( NXOpen.CAE.LbcAssociationMgrBcType
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
ExportToCsv¶
-
LbcAssociationMgr.
ExportToCsv
¶ Export to csv
Signature
ExportToCsv(csvFileName)
Parameters: csvFileName (str) – CSV file name NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: None.
ImportFromCsv¶
-
LbcAssociationMgr.
ImportFromCsv
¶ Import from csv
Signature
ImportFromCsv(csvFileName)
Parameters: csvFileName (str) – CSV file name NOTE: The full Unicode character set is not supported for this parameter. New in version NX10.0.0.
License requirements: None.
Validate¶
-
LbcAssociationMgr.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.