SimBCBuilder Class¶
-
class
NXOpen.CAE.
SimBCBuilder
¶ Bases:
NXOpen.NXObject
This is a manager to the
CAE.SimBC
class. Objects of typeCAE.SimBC
can be created and edited only through this classNew in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Bc | Returns the CAE.SimBC object |
BcLabel | Returns or sets the label of CAE.SimBC object |
BcName | Returns or sets the name of CAE.SimBC object |
DestinationFolder | Returns or sets the destination folder of CAE.SimBC object |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PropertyTable | Returns the property table for the CAE.SimBC object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
TargetSetManager | Returns the target set manager for CAE.SimBC object |
Methods¶
Method | Description |
---|---|
CommitAddBc | Commits the creation of the CAE.SimBC objects or Commits the changes made to the CAE.SimBC and adds the BC to the current active solution/step @return boundary condition |
CommitBc | Commits the creation of the CAE.SimBC objects or Commits the changes made to the CAE.SimBC @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
Bc¶
-
SimBCBuilder.
Bc
¶ Returns the
CAE.SimBC
object-------------------------------------
Getter Method
Signature
Bc()
Returns: boundary condition Return type: NXOpen.CAE.SimBC
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BcLabel¶
-
SimBCBuilder.
BcLabel
¶ Returns or sets the label of
CAE.SimBC
object-------------------------------------
Getter Method
Signature
BcLabel()
Returns: label of the bc Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
BcLabel(label)
Parameters: label (int) – label of the bc New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
BcName¶
-
SimBCBuilder.
BcName
¶ Returns or sets the name of
CAE.SimBC
object-------------------------------------
Getter Method
Signature
BcName()
Returns: name of the bc Return type: str New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
BcName(name)
Parameters: name (str) – name of the bc New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DestinationFolder¶
-
SimBCBuilder.
DestinationFolder
¶ Returns or sets the destination folder of
CAE.SimBC
object-------------------------------------
Getter Method
Signature
DestinationFolder()
Returns: destination folder Return type: NXOpen.CAE.SimLbcFolder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
DestinationFolder(folder)
Parameters: folder ( NXOpen.CAE.SimLbcFolder
) – destination folderNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
SimBCBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SimBCBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SimBCBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SimBCBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SimBCBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PropertyTable¶
-
SimBCBuilder.
PropertyTable
¶ Returns the property table for the
CAE.SimBC
object-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: property table Return type: NXOpen.CAE.PropertyTable
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
SimBCBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
TargetSetManager¶
-
SimBCBuilder.
TargetSetManager
¶ Returns the target set manager for
CAE.SimBC
object-------------------------------------
Getter Method
Signature
TargetSetManager()
Returns: target set manager Return type: NXOpen.CAE.SetManager
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
CommitAddBc¶
-
SimBCBuilder.
CommitAddBc
¶ Commits the creation of the
CAE.SimBC
objects or Commits the changes made to theCAE.SimBC
and adds the BC to the current active solution/stepSignature
CommitAddBc()
Returns: boundary condition Return type: NXOpen.CAE.SimBC
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CommitBc¶
-
SimBCBuilder.
CommitBc
¶ Commits the creation of the
CAE.SimBC
objects or Commits the changes made to theCAE.SimBC
Signature
CommitBc()
Returns: Return type: NXOpen.CAE.SimBC
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Destroy¶
-
SimBCBuilder.
Destroy
¶ Deletes the builder, and cleans up any objects created by the builder.
This method should always be called when create/edit of the BC object is completed
Signature
Destroy()
New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimBCBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
SimBCBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SimBCBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.