AlignmentMethodBuilder Class |
Represents a NXOpen.GeometricUtilities.AlignmentMethodBuilder |
AlongPathPattern Class |
the AlongPath pattern definition. |
AlongSpineBuilder Class |
Represents a NXOpen.GeometricUtilities.AlongSpineBuilder |
AnchorLocatorBuilder Class |
Represents a NXOpen.GeometricUtilities.AnchorLocatorBuilder |
AngularLimits Class |
Represents a angular limts data. |
AngularPatternSpacing Class |
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class. |
BetweenLocationsData Class |
Represents a NXOpen.GeometricUtilities.BetweenLocationsData |
BlendLimitsData Class |
Represents a NXOpen.GeometricUtilities.BlendLimitsData |
BlendSetbackBuilder Class |
This class provides ability to define a setback curve on a blend face. |
BlendSetbackBuilderList Class |
Represents a list of objects. |
BlendStopshortBuilder Class |
Represents a NXOpen.GeometricUtilities.BlendStopshortBuilder |
BlendStopshortBuilderCollection Class |
This class contains the factory methods for creating an BlendStopshortBuilder. |
BooleanOperation Class |
Represents a boolean operation . |
BooleanRegionSelect Class |
a class which defines boolean region select. |
BooleanToolBuilder Class |
a class which defines boolean tool builder. |
BoundaryDefinitionBuilder Class |
Represents a NXOpen.GeometricUtilities.BoundaryDefinitionBuilder . |
BoundaryDefinitionBuilderList Class |
Represents a list of objects. |
BoundingObjectBuilder Class |
Represents a NXOpen.GeometricUtilities.BoundingObjectBuilder |
BoundingObjectBuilderList Class |
Represents a list of objects. |
BridgeCurveConnectivity Class |
Data offering connectivity controls for NXOpen.Features.BridgeCurveBuilderEx . |
CAMDataPrepManager Class |
Contains the create functions for builders. |
CircularCrossSection Class |
Represents a circular section data for face blend. |
CircularFrameBuilder Class |
Represents a NXOpen.GeometricUtilities.CircularFrameBuilder |
CircularPattern Class |
the circular pattern definition. |
ColorCodedRegionBuilder Class |
Represents a NXOpen.GeometricUtilities.ColorCodedRegionBuilder . |
CombOptionsBuilder Class |
Represents a NXOpen.GeometricUtilities.CombOptionsBuilder |
ConicCrossSection Class |
Represents a conic section data for face blend. |
Continuity Class |
Represents a NXOpen.GeometricUtilities.Continuity Allows user to specify continuity constraint surface construction. |
ControlPoleManagerData Class |
This class manages the control poles for a set of surfaces or curves. |
ConvertFeatureGroupsToModulesBuilder Class |
Represents a NXOpen.GeometricUtilities.ConvertFeatureGroupsToModulesBuilder builder |
CurveExtendData Class |
Represents a NXOpen.GeometricUtilities.CurveExtendData |
CurveExtensionBuilder Class |
Spline extension builder class. |
CurveFitData Class |
Represents the curve fitting methods options. |
CurveFitJoin Class |
Represents the curve fit join data |
CurveFitOptions Class |
Represents the curve fit data |
CurveLengthData Class |
Represents an CurveLength data. |
CurveLimitsData Class |
Represents a NXOpen.GeometricUtilities.CurveLimitsData |
CurveOptions Class |
Represents the curve options data |
CurveRangeBuilder Class |
Represents the curve range and anchor builder |
CurveSettings Class |
Represents the curve settings data |
CurveShapingBuilder Class |
Represents a NXOpen.GeometricUtilities.CurveShapingBuilder . |
DegreesAndSegmentsOrPatchesBuilder Class |
the DegreesAndSegmentsOrPatches builder |
DepthSkewBuilder Class |
This class provides ability to specify a depth and a skew value. |
DisplayResolutionBuilder Class |
Represents a NXOpen.GeometricUtilities.DisplayResolutionBuilder . |
DistancePatternSpacing Class |
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class. |
DraftPointData Class |
Represents a draft point data object |
DraftVariableAngleData Class |
Represents data containing variable angle draft point data objects |
EndHoleData Class |
Represents a NXOpen.GeometricUtilities.EndHoleData |
EntityUsageInfo Class |
Represents a NXOpen.GeometricUtilities.EntityUsageInfo . |
EntityUsageInfoList Class |
Represents a list of objects. |
EnumTest Class |
Represents a GeometricUtilities.EnumTest |
Extend Class |
Represents an extend data. |
ExtrudeRevolveToolBuilder Class |
a class which is a sub-component of BooleanTool. |
FaceChangeOverflowBehavior Class |
Represents a NXOpen.GeometricUtilities.FaceChangeOverflowBehavior It provides several face change options for controlling behavior when a change face overflows an incident face. |
FacePlaneSelectionBuilder Class |
Represents a NXOpen.GeometricUtilities.FacePlaneSelectionBuilder |
FacePlaneSelectionBuilderCollection Class |
This class contains the factory methods for creating an FacePlaneSelectionBuilder. |
FacePlaneToolBuilder Class |
a sub-component of BooleanToolBuilder. |
FaceSetData Class |
Represents a NXOpen.GeometricUtilities.FaceSetData |
FaceSetDataCollection Class |
This class contains the factory methods for creating an FaceSetData. |
FaceSetOffset Class |
This class represents a face set (collector) offset data. |
FaceSetOffsetCollection Class |
This class contains the factory methods for creating an face set offset. |
FaceSetOffsetList Class |
Represents a list of objects. |
FeatureOffset Class |
Represents a Offset . |
FeatureOptions Class |
Represents various options supported on features. |
FlowDirection Class |
Represents a NXOpen.GeometricUtilities.FlowDirection Allows user to specify different flow direction to control output surface shape. |
FrameOnPathBuilder Class |
Frame on path builder |
FtmFixedCurvesBuilder Class |
Represents a NXOpen.GeometricUtilities.FtmFixedCurvesBuilder builder |
FtmFixedCurvesBuilderList Class |
Represents a list of objects. |
FtmTransformCurvesBuilder Class |
Represents a NXOpen.GeometricUtilities.FtmTransformCurvesBuilder builder |
FtmTransformCurvesBuilderList Class |
Represents a list of objects. |
FtmTransformPointsBuilder Class |
Represents a NXOpen.GeometricUtilities.FtmTransformPointsBuilder builder |
FtmTransformPointsBuilderList Class |
Represents a list of objects. |
GeneralPattern Class |
the General pattern definition. |
GeometryLocationData Class |
Represents a NXOpen.GeometricUtilities.GeometryLocationData |
GeometryLocationDataCollection Class |
This class contains the factory methods for creating GeometryLocationData. |
HelixPattern Class |
the Helix pattern definition. |
HorizontalReference Class |
the horizontal reference vector definition. |
IComponentBuilder Class |
Represents a component contained in a builder |
InstanceEditedExpressionItem Class |
edited value of one master expression of the input object(s) being patterned. |
InstanceEditedExpressionItemList Class |
Represents a list of objects. |
InstanceEditedExpressionsList Class |
list of NXOpen.GeometricUtilities.InstanceEditedExpressionItem objects. |
InteractiveSectionBuilder Class |
Represents a NXOpen.GeometricUtilities.InteractiveSectionBuilder . |
LawBuilder Class |
Represents a LawBuilder |
Limits Class |
Represents a limits data. |
LinearLimits Class |
Represents a limits data. |
LocalUntrimBuilder Class |
Represents a NXOpen.GeometricUtilities.LocalUntrimBuilder builder. |
LocalUntrimManager Class |
Provides create builder methods for LocalUntrimBuilder |
MatchSurfaceBuilder Class |
Represents a NXOpen.GeometricUtilities.MatchSurfaceBuilder builder. |
MiddleHoleData Class |
Represents a NXOpen.GeometricUtilities.MiddleHoleData |
MirrorPattern Class |
the Mirror pattern definition. |
ModlAlongCurveAngle Class |
This class NXOpen.GeometricUtilities.ModlAlongCurveAngle represents motion type in ModlMotion |
ModlDistanceAngle Class |
Represents a NXOpen.GeometricUtilities.ModlDistanceAngle |
ModlMotion Class |
Represents a NXOpen.GeometricUtilities.ModlMotion |
MovePoleBuilder Class |
This class manages the control poles movements for a surface or curve. |
MultiDraft Class |
Represents a multi-draft. |
MultiTransitionLawBuilder Class |
Represents multiple transition law. |
NestModuleBuilder Class |
Represents a NXOpen.GeometricUtilities.NestModuleBuilder |
NonInflectingLawBuilder Class |
Represents a non-inflecting law. |
OmnicadManager Class |
Represents a manager for creating builder objects for OmniCAD Free Transformer |
OnPathDimWithValueBuilder Class |
Represents a NXOpen.GeometricUtilities.OnPathDimWithValueBuilder |
OnPathDimensionBuilder Class |
Builds an on-path dimension |
OnPathDistancePatternSpacing Class |
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class. |
OrientXpressBuilder Class |
Represent the OrientXpress block |
OrientXpressTestBuilder Class |
Represents a ModlUtilsJA.OrientXpressTest builder |
OrientationMethodBuilder Class |
Represents a NXOpen.GeometricUtilities.OrientationMethodBuilder |
ParentEquivalencyMap Class |
Represents a NXOpen.GeometricUtilities.ParentEquivalencyMap . |
ParentEquivalencyMapList Class |
Represents a list of objects. |
PartModuleInputBuilder Class |
Represents a NXOpen.GeometricUtilities.PartModuleInputBuilder |
PartModuleOutputBuilder Class |
Represents a NXOpen.GeometricUtilities.PartModuleOutputBuilder |
PartModuleOutputBuilder1 Class |
Represents a NXOpen.GeometricUtilities.PartModuleOutputBuilder1 |
PartModuleReferencesBuilder Class |
Represents a NXOpen.GeometricUtilities.PartModuleReferencesBuilder |
PartModuleRelationshipBuilder Class |
Represents a Features.PartModule builder |
PathLimits Class |
Represents a path limits data. |
PatternClocking Class |
enables the ability to apply delta transforms on individual instances of a pattern |
PatternClockingBuilder Class |
enables the ability to apply delta transforms on individual instances of a pattern within the pattern feature |
PatternDefinition Class |
pattern spacing for several pattern based commands. |
PatternFill Class |
the pattern fill definition. |
PatternIncrementItem Class |
variational for one master expression of the input object(s) being patterned. |
PatternIncrementItemList Class |
Represents a list of objects. |
PatternIncrementsBuilder Class |
pattern increments builder |
PatternIncrementsList Class |
list of NXOpen.GeometricUtilities.PatternIncrementItem objects. |
PatternInstanceEditBuilder Class |
pattern instance edit builder |
PatternOrientation Class |
the pattern orientation definition. |
PatternReferencePointServiceBuilder Class |
Pattern Reference Point is a service which enables the employing client to compute the reference point for pattern instance locations. |
PatternSpacing Class |
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class. |
PatternSpacingsList Class |
list of NXOpen.GeometricUtilities.PatternSpacingsListItem objects. |
PatternSpacingsListItem Class |
one pattern spacing in the spacings list |
PatternSpacingsListItemList Class |
Represents a list of objects. |
PlayButtonsBuilder Class |
VCR buttons for any dialog that needs them |
PointSetAlignmentBuilder Class |
This class performs a point set to point set alignment |
PointsFromFileBuilder Class |
Represents a NXOpen.GeometricUtilities.PointsFromFileBuilder builder read points from a text file with format *. |
PolygonPattern Class |
the polygon pattern definition. |
PolygonPatternSpacing Class |
defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class. |
ProjectionOptions Class |
Represents a ProjectionOptions |
QuadrilateralFrameBuilder Class |
Represents a NXOpen.GeometricUtilities.QuadrilateralFrameBuilder |
Rebuild Class |
Represents a NXOpen.GeometricUtilities.Rebuild . |
RectangularFrameBuilder Class |
Rectangular frame builder |
RectangularPattern Class |
the rectangular pattern definition. |
ReduceSurfaceRadiusBuilder Class |
Reduce Surface Radius Builder of Geometric Utilities. |
ReduceSurfaceRadiusFaceGroupBuilder Class |
Reduce Surface Radius Face Group Builder of Geometric Utilities. |
ReduceSurfaceRadiusFaceGroupBuilderList Class |
Represents a list of objects. |
ReferencePattern Class |
the reference pattern definition. |
RefitControlBuilder Class |
This class is used to specify the parameter set to refit faces |
RegionTracker Class |
a class which collects all the geometric entities used to identify a region of faces during a boolean feature. |
RenameLinkedPartModulePartBuilder Class |
Represents a Features.PartModule builder |
RenewFeatureBuilder Class |
Represents a RenewFeatureBuilder object. |
ReplAsstBuilder Class |
Represents a NXOpen.GeometricUtilities.ReplAsstBuilder . |
RotationSetBuilder Class |
Represents a NXOpen.GeometricUtilities.RotationSetBuilder |
RotationSetBuilderList Class |
Represents a list of objects. |
SShapedLawBuilder Class |
Represents a s-shaped law. |
SaveConstraintsBuilder Class |
Represents a builder for a Save Constraints. |
ScalingMethodBuilder Class |
Represents a NXOpen.GeometricUtilities.ScalingMethodBuilder |
ScalingSetBuilder Class |
Represents a NXOpen.GeometricUtilities.ScalingSetBuilder |
ScalingSetBuilderList Class |
Represents a list of objects. |
SecondarySectionData Class |
Represents a NXOpen.GeometricUtilities.SecondarySectionData |
SectionPlaneData Class |
Represents a Section Plane Data class This class acts like a container to hold the data needed to create a plane. |
SelectDividingObjectBuilder Class |
Represents the dividing tool block for dividing face |
SelectionList Class |
Represents a NXOpen.GeometricUtilities.SelectionList |
SelectionListList Class |
Represents a list of objects. |
ShapeFrameBuilder Class |
Represents a NXOpen.GeometricUtilities.ShapeFrameBuilder |
SimpleDraft Class |
Represents an Offset . |
SmartVolumeProfileBuilder Class |
This class contains the options for automatically closing the profile to surrounding model geometry. |
SnipIntoPatchesBuilder Class |
Represents a NXOpen.GeometricUtilities.SnipIntoPatchesBuilder builder. |
SpineDefinitionBuilder Class |
Provides a spine definition for modeling operations |
SpinePlaneBuilder Class |
Represents a NXOpen.GeometricUtilities.SpinePlaneBuilder . |
SpinePlaneBuilderList Class |
Represents a list of objects. |
SpinePointData Class |
Represents a spine point def object |
SpinePointDataCollection Class |
This class contains the factory methods for creating a SpinePointData object. |
SpiralPattern Class |
the Spiral pattern definition. |
SplineExtensionBuilder Class |
Spline extension builder class. |
StartHoleData Class |
Represents a NXOpen.GeometricUtilities.StartHoleData |
StepOptionBehavior Class |
Represents a NXOpen.GeometricUtilities.StepOptionBehavior It provides several step options for controlling behavior when move face and so on. |
StringTestBuilder Class |
Represents a StringTestBuilder |
StyledSweepDoubleOnPathDimBuilder Class |
Represents a NXOpen.GeometricUtilities.StyledSweepDoubleOnPathDimBuilder |
StyledSweepDoubleOnPathDimBuilderList Class |
Represents a list of objects. |
StyledSweepReferenceMethodBuilder Class |
Represents a NXOpen.GeometricUtilities.StyledSweepReferenceMethodBuilder |
SupportPlaneData Class |
Represents a NXOpen.GeometricUtilities.SupportPlaneData |
SurfaceRangeBuilder Class |
Represents the surface range and anchor builder |
TangentMagnitudeBuilder Class |
This class provides ability to specify the start and end tangent magnitude values. |
TransformerData Class |
Transformation and orientation tool. |
TransitionCurveBuilder Class |
This class provides ability to create a transition(bridge) curve between two adjacent setback curves. |
TransitionCurveBuilderList Class |
Represents a list of objects. |
TransitionLawNodeBuilder Class |
Represents a law node with transition type. |
TransitionLawNodeBuilderList Class |
Represents a list of objects. |
TriangularFrameBuilder Class |
Represents a NXOpen.GeometricUtilities.TriangularFrameBuilder |
TwoExpressionsCollectorSet Class |
Represents a two dimension list item builder |
TwoExpressionsCollectorSetList Class |
Represents a list of objects. |
TwoExpressionsSectionSet Class |
Represents a two dimension list section item builder |
TwoExpressionsSectionSetList Class |
Represents a list of objects. |
UnnestModuleBuilder Class |
Represents a NXOpen.GeometricUtilities.UnnestModuleBuilder |
ValueTestBuilder Class |
Represents a ValueTestBuilder |
WaveLinkRepository Class |
Represents a NXOpen.GeometricUtilities.WaveLinkRepository . |