EnumTestTrees Enumeration¶
NXOpen.GeometricUtilities.EnumTest.Trees is an alias for NXOpen.GeometricUtilities.EnumTestTrees
-
class
NXOpen.GeometricUtilities.
EnumTestTrees
¶ Bases:
object
Trees can taste pretty good but have a rather barky texture
Enum Members
Enum Member Enum Member Description Willow willows are fluffyPine pine cones are not fluffyGingko gingko helps your brain-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-