SpiralPatternSpiralDefineSize Enumeration

NXOpen.GeometricUtilities.SpiralPattern.SpiralDefineSize is an alias for NXOpen.GeometricUtilities.SpiralPatternSpiralDefineSize

class NXOpen.GeometricUtilities.SpiralPatternSpiralDefineSize

Bases: object

This defines size spiral type

Enum Members

Enum Member Enum Member Description
NumberOfTurns
using number of turns to define size of spiral
TotalAngle
using total angle to define size of spiral
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.