PatternReferencePointServiceBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PatternReferencePointServiceBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Pattern Reference Point is a service which enables the employing client to compute the reference point for pattern instance locations.
The reference point can be inferred or user-selected .. versionadded:: NX9.0.0
Properties¶
Property | Description |
---|---|
IsReferencePointInferred | Returns or sets the reference point inferred flag. |
Point | Returns or sets the reference point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IsReferencePointInferred¶
-
PatternReferencePointServiceBuilder.
IsReferencePointInferred
¶ Returns or sets the reference point inferred flag.
This flag states whether the reference point is inferred from selected entites or not. If ‘true’, the reference point will be inferred every time the selected entities get modified or updated. If ‘false’, the reference point provided by the user will be independent of the selected entities but will be associative to the rule by which it was created (e.g. End of Line, Center of Arc).
-------------------------------------
Getter Method
Signature
IsReferencePointInferred()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsReferencePointInferred(isReferencePointInferred)
Parameters: isReferencePointInferred (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Point¶
-
PatternReferencePointServiceBuilder.
Point
¶ Returns or sets the reference point
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
PatternReferencePointServiceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.