TangentMagnitudeBuilder Class

class NXOpen.GeometricUtilities.TangentMagnitudeBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

This class provides ability to specify the start and end tangent magnitude values.

New in version NX6.0.0.

Properties

Property Description
EndTangentMagnitude Returns the end tangent magnitude
StartTangentMagnitude Returns the start tangent magnitude
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

EndTangentMagnitude

TangentMagnitudeBuilder.EndTangentMagnitude

Returns the end tangent magnitude

-------------------------------------

Getter Method

Signature EndTangentMagnitude()

Returns:
Return type:NXOpen.Expression

New in version NX6.0.0.

License requirements: None.

StartTangentMagnitude

TangentMagnitudeBuilder.StartTangentMagnitude

Returns the start tangent magnitude

-------------------------------------

Getter Method

Signature StartTangentMagnitude()

Returns:
Return type:NXOpen.Expression

New in version NX6.0.0.

License requirements: None.

Method Detail

Validate

TangentMagnitudeBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.