PatternSpacingSpacingType Enumeration

NXOpen.GeometricUtilities.PatternSpacing.SpacingType is an alias for NXOpen.GeometricUtilities.PatternSpacingSpacingType

class NXOpen.GeometricUtilities.PatternSpacingSpacingType

Bases: object

defines the type of spacing instances can have within a pattern.

Enum Members

Enum Member Enum Member Description
Offset
Specify distance from the origin of one instance to the origin of the next instance.
Span
Specify a distance for which all instances should occupy.
PitchAndSpan
Specify distance between instances and distance for all instances, number of copies is calculated.
Pitch
This is for pattern fill case. Count is calculated based on the pitch and fill boundary box.
List
Specify offsets with a list.
PolygonCountPerSide
This is for Polygon type. Specify number of count per side.
PolygonPitchAlongSide
This is for Polygon type. Specify a pitch distance along one side.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.