AlignmentMethodBuilder Class¶
-
class
NXOpen.GeometricUtilities.
AlignmentMethodBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.AlignmentMethodBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AlignAxis | Returns or sets the alignment axis |
AlignCurve | Returns the align curve |
AlignType | Returns or sets the alignment type |
AlignVector | Returns or sets the alignment vector |
EndAlignFillerSurfaceOption | Returns or sets the end align filler surface option |
NumberOfPointsPerSection | Returns the number of alignment points in each section. |
NumberOfSections | Returns the number of section in the alignment point block |
StartAlignFillerSurfaceOption | Returns or sets the start align filler surface option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddPoint | Insert a given point, and create corresponding points on other sections. |
AddSection | Add a section at the given index among existing sections. |
ComputeDefaultPoints | Calculate default alignment points on existing sections. |
CreateOnPathDimBuilder | Set the sections. |
GetAllPoints | Get all of the alignment points, returns as a single dimension array @return Gets all the points, numPoints is total number of points, not points per section |
GetPoint | Gets an alignment point for a section @return |
RemoveAllPoints | Remove all alignment points. |
RemovePoint | Remove given point, also remove corresponding points on other sections |
RemoveSection | Find and delete the section |
RemoveSectionAtIndex | Remove section at given index |
SetAlignPoints | Set the Alignment Points when sections have been set up. |
SetSections | Set the sections. |
UnloadSections | Unload sections held by the builder |
UpdateSectionAtIndex | Update section at given index |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AlignmentMethodBuilderAlignFillerSurfaceType Enumeration | Filler surface types |
AlignmentMethodBuilderType Enumeration | Alignment types supported |
Property Detail¶
AlignAxis¶
-
AlignmentMethodBuilder.
AlignAxis
¶ Returns or sets the alignment axis
-------------------------------------
Getter Method
Signature
AlignAxis()
Returns: Return type: NXOpen.Axis
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignAxis(alignAxis)
Parameters: alignAxis ( NXOpen.Axis
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AlignCurve¶
-
AlignmentMethodBuilder.
AlignCurve
¶ Returns the align curve
-------------------------------------
Getter Method
Signature
AlignCurve()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
AlignType¶
-
AlignmentMethodBuilder.
AlignType
¶ Returns or sets the alignment type
-------------------------------------
Getter Method
Signature
AlignType()
Returns: Return type: NXOpen.GeometricUtilities.AlignmentMethodBuilderType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignType(alignType)
Parameters: alignType ( NXOpen.GeometricUtilities.AlignmentMethodBuilderType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AlignVector¶
-
AlignmentMethodBuilder.
AlignVector
¶ Returns or sets the alignment vector
-------------------------------------
Getter Method
Signature
AlignVector()
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignVector(alignVector)
Parameters: alignVector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EndAlignFillerSurfaceOption¶
-
AlignmentMethodBuilder.
EndAlignFillerSurfaceOption
¶ Returns or sets the end align filler surface option
-------------------------------------
Getter Method
Signature
EndAlignFillerSurfaceOption()
Returns: Return type: NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndAlignFillerSurfaceOption(fillerSurfaceType)
Parameters: fillerSurfaceType ( NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
NumberOfPointsPerSection¶
-
AlignmentMethodBuilder.
NumberOfPointsPerSection
¶ Returns the number of alignment points in each section.
All the sections always have same number of alignment points
-------------------------------------
Getter Method
Signature
NumberOfPointsPerSection()
Returns: Number of alignment points in each section Return type: int New in version NX5.0.1.
License requirements: None.
NumberOfSections¶
-
AlignmentMethodBuilder.
NumberOfSections
¶ Returns the number of section in the alignment point block
-------------------------------------
Getter Method
Signature
NumberOfSections()
Returns: Number of sections Return type: int New in version NX5.0.1.
License requirements: None.
StartAlignFillerSurfaceOption¶
-
AlignmentMethodBuilder.
StartAlignFillerSurfaceOption
¶ Returns or sets the start align filler surface option
-------------------------------------
Getter Method
Signature
StartAlignFillerSurfaceOption()
Returns: Return type: NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartAlignFillerSurfaceOption(fillerSurfaceType)
Parameters: fillerSurfaceType ( NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
AddPoint¶
-
AlignmentMethodBuilder.
AddPoint
¶ Insert a given point, and create corresponding points on other sections.
The points on other sections are computed based on existing alignment points
Signature
AddPoint(alignPoint)
Parameters: alignPoint ( NXOpen.GeometricUtilities.OnPathDimensionBuilder
) – Pt to insertReturns: Index of the newly added point on each section Return type: int New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
AddSection¶
-
AlignmentMethodBuilder.
AddSection
¶ Add a section at the given index among existing sections.
Computes points for other sections
Signature
AddSection(sectionIndex, sec)
Parameters: - sectionIndex (int) – Where to insert. New section will have this index
- sec (
NXOpen.Section
) – The New section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ComputeDefaultPoints¶
-
AlignmentMethodBuilder.
ComputeDefaultPoints
¶ Calculate default alignment points on existing sections.
Pre-existing alignment points destroyed
Signature
ComputeDefaultPoints()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CreateOnPathDimBuilder¶
-
AlignmentMethodBuilder.
CreateOnPathDimBuilder
¶ Set the sections.
Does not compute default alignment
Signature
CreateOnPathDimBuilder(sec, pnt)
Parameters: - sec (
NXOpen.Section
) – The section on which to create the builder - pnt (
NXOpen.Point3d
) – The point on the section
Returns: The generated onPathDim
Return type: New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- sec (
GetAllPoints¶
-
AlignmentMethodBuilder.
GetAllPoints
¶ Get all of the alignment points, returns as a single dimension array
Signature
GetAllPoints()
Returns: a tuple Return type: A tuple consisting of (alignPoints, numSection). alignPoints is a list of NXOpen.GeometricUtilities.OnPathDimensionBuilder
. Gets all the points, numPoints is total number of points, not points per section numSection is a int. Number of sections returnedNew in version NX5.0.0.
License requirements: None.
GetPoint¶
-
AlignmentMethodBuilder.
GetPoint
¶ Gets an alignment point for a section
Signature
GetPoint(sectionIndex, pointIndex)
Parameters: - sectionIndex (int) – Section on which to query the alignment point
- pointIndex (int) – Alignment point index
Returns: Return type: New in version NX5.0.1.
License requirements: None.
RemoveAllPoints¶
-
AlignmentMethodBuilder.
RemoveAllPoints
¶ Remove all alignment points.
Keeps the sections
Signature
RemoveAllPoints()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemovePoint¶
-
AlignmentMethodBuilder.
RemovePoint
¶ Remove given point, also remove corresponding points on other sections
Signature
RemovePoint(alignPoint)
Parameters: alignPoint ( NXOpen.GeometricUtilities.OnPathDimensionBuilder
) – Pt do deleteNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveSection¶
-
AlignmentMethodBuilder.
RemoveSection
¶ Find and delete the section
Signature
RemoveSection(sec)
Parameters: sec ( NXOpen.Section
) – Existing section within the AlignmentNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveSectionAtIndex¶
-
AlignmentMethodBuilder.
RemoveSectionAtIndex
¶ Remove section at given index
Signature
RemoveSectionAtIndex(secIndex)
Parameters: secIndex (int) – The index of the section to remove New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetAlignPoints¶
-
AlignmentMethodBuilder.
SetAlignPoints
¶ Set the Alignment Points when sections have been set up.
The incoming points are organized section by section. The points parent section match the pre-existing sections held by this object
Signature
SetAlignPoints(alignPoints)
Parameters: alignPoints (list of NXOpen.GeometricUtilities.OnPathDimensionBuilder
) – Sets the points on the section, numPoints is total number of points for all sectionsNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetSections¶
-
AlignmentMethodBuilder.
SetSections
¶ Set the sections.
Does not compute default alignment
Signature
SetSections(sections)
Parameters: sections (list of NXOpen.Section
) – Array of sectionsNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UnloadSections¶
-
AlignmentMethodBuilder.
UnloadSections
¶ Unload sections held by the builder
Signature
UnloadSections()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpdateSectionAtIndex¶
-
AlignmentMethodBuilder.
UpdateSectionAtIndex
¶ Update section at given index
Signature
UpdateSectionAtIndex(secIndex)
Parameters: secIndex (int) – The index of the section to remove New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
AlignmentMethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.