AlignmentMethodBuilderAlignFillerSurfaceType Enumeration

NXOpen.GeometricUtilities.AlignmentMethodBuilder.AlignFillerSurfaceType is an alias for NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType

class NXOpen.GeometricUtilities.AlignmentMethodBuilderAlignFillerSurfaceType

Bases: object

Filler surface types

Enum Members

Enum Member Enum Member Description
NoFiller
No end filler surface
Cone Generalized conical developable surface.
Cylinder Generalized cylindrical developable surface.
Trimmed Trimmed developable surface.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.