PointSetAlignmentBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PointSetAlignmentBuilder
¶ Bases:
NXOpen.Builder
This class performs a point set to point set alignment
To create a new instance of this class, use
NXOpen.Part.CreatePointSetAlignmentBuilder()
Default values.
Property Value Constraint None New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Constraint | Returns or sets the constraint |
FromPointSet | Returns the from point set |
ObjectsToMove | Returns the objects to move |
Tag | Returns the Tag for this object. |
ToPointSet | Returns the to point set |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PointSetAlignmentBuilderConstraintOptions Enumeration | Constraint Options |
Property Detail¶
Constraint¶
-
PointSetAlignmentBuilder.
Constraint
¶ Returns or sets the constraint
-------------------------------------
Getter Method
Signature
Constraint()
Returns: Return type: NXOpen.GeometricUtilities.PointSetAlignmentBuilderConstraintOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Constraint(constraint)
Parameters: constraint ( NXOpen.GeometricUtilities.PointSetAlignmentBuilderConstraintOptions
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FromPointSet¶
-
PointSetAlignmentBuilder.
FromPointSet
¶ Returns the “from” point set
-------------------------------------
Getter Method
Signature
FromPointSet()
Returns: Return type: NXOpen.SelectPointList
New in version NX7.5.0.
License requirements: None.
ObjectsToMove¶
-
PointSetAlignmentBuilder.
ObjectsToMove
¶ Returns the objects to move
-------------------------------------
Getter Method
Signature
ObjectsToMove()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
ToPointSet¶
-
PointSetAlignmentBuilder.
ToPointSet
¶ Returns the “to” point set
-------------------------------------
Getter Method
Signature
ToPointSet()
Returns: Return type: NXOpen.SelectPointList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
PointSetAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.