BetweenLocationsData Class¶
-
class
NXOpen.GeometricUtilities.
BetweenLocationsData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.BetweenLocationsData
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FromLocation | Returns the from location |
Tag | Returns the Tag for this object. |
ToLocationList | Returns the to location list |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FromLocation¶
-
BetweenLocationsData.
FromLocation
¶ Returns the from location
-------------------------------------
Getter Method
Signature
FromLocation()
Returns: Return type: NXOpen.GeometricUtilities.GeometryLocationData
New in version NX5.0.0.
License requirements: None.
ToLocationList¶
-
BetweenLocationsData.
ToLocationList
¶ Returns the to location list
-------------------------------------
Getter Method
Signature
ToLocationList()
Returns: Return type: NXOpen.TaggedObjectList
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BetweenLocationsData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.