ScalingMethodBuilder Class

class NXOpen.GeometricUtilities.ScalingMethodBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.ScalingMethodBuilder

New in version NX5.0.0.

Properties

Property Description
AreaLaw Returns the area law.
BlendingFunctionType Returns or sets the blending function.
EndBlendScaleFactor Returns or sets the end blend scale factor.
PerimeterLaw Returns the perimeter law.
ScaleFactor Returns or sets the scale factor.
ScalingCurve Returns the scaling curve.
ScalingOption Returns or sets the scaling method option.
ScalingPoint Returns or sets the scaling point.
StartBlendScaleFactor Returns or sets the start blend scale factor.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

ScalingMethodBuilderBlendingFunctionTypes Enumeration This enum represents the blending function type, if the scaling by BlendingFunction is selected.
ScalingMethodBuilderScalingOptions Enumeration This enum represents the scaling method option.

Property Detail

AreaLaw

ScalingMethodBuilder.AreaLaw

Returns the area law.

For scaling by Area Law, the input law governs the cross sectional area at the start and end of the guide curve.

-------------------------------------

Getter Method

Signature AreaLaw()

Returns:
Return type:NXOpen.GeometricUtilities.LawBuilder

New in version NX5.0.0.

License requirements: None.

BlendingFunctionType

ScalingMethodBuilder.BlendingFunctionType

Returns or sets the blending function.

Allows linear or cubic scaling between specified starting and ending scale factors, which correspond to the start and end of the guide string.

-------------------------------------

Getter Method

Signature BlendingFunctionType()

Returns:
Return type:NXOpen.GeometricUtilities.ScalingMethodBuilderBlendingFunctionTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature BlendingFunctionType(blendingFunctionType)

Parameters:blendingFunctionType (NXOpen.GeometricUtilities.ScalingMethodBuilderBlendingFunctionTypes) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

EndBlendScaleFactor

ScalingMethodBuilder.EndBlendScaleFactor

Returns or sets the end blend scale factor.

For scaling by Blending Function, the end scale factor will be applied at the end point of the guide curve.

-------------------------------------

Getter Method

Signature EndBlendScaleFactor()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EndBlendScaleFactor(endBlendScaleFactor)

Parameters:endBlendScaleFactor (float) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

PerimeterLaw

ScalingMethodBuilder.PerimeterLaw

Returns the perimeter law.

For scaling by Perimeter Law, the input law governs the perimeter of the sections at the start and end of the guide curve.

-------------------------------------

Getter Method

Signature PerimeterLaw()

Returns:
Return type:NXOpen.GeometricUtilities.LawBuilder

New in version NX5.0.0.

License requirements: None.

ScaleFactor

ScalingMethodBuilder.ScaleFactor

Returns or sets the scale factor.

For Constant scaling method, the scale factor will be applied to all sections along the guide.

-------------------------------------

Getter Method

Signature ScaleFactor()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScaleFactor(scaleFactor)

Parameters:scaleFactor (float) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

ScalingCurve

ScalingMethodBuilder.ScalingCurve

Returns the scaling curve.

For scaling by Another Curve, the scale at any given point is based on the length of the ruling between the guide string and the input scaling curve.

-------------------------------------

Getter Method

Signature ScalingCurve()

Returns:
Return type:NXOpen.Section

New in version NX5.0.0.

License requirements: None.

ScalingOption

ScalingMethodBuilder.ScalingOption

Returns or sets the scaling method option.

Except for Uniform and Lateral scaling methods, additional parameters and/or inputs are required.

-------------------------------------

Getter Method

Signature ScalingOption()

Returns:
Return type:NXOpen.GeometricUtilities.ScalingMethodBuilderScalingOptions

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScalingOption(scalingOption)

Parameters:scalingOption (NXOpen.GeometricUtilities.ScalingMethodBuilderScalingOptions) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

ScalingPoint

ScalingMethodBuilder.ScalingPoint

Returns or sets the scaling point.

For scaling by a Point, the scale at any given point is based on the length of the ruling between the guide string and the input point.

-------------------------------------

Getter Method

Signature ScalingPoint()

Returns:
Return type:NXOpen.Point

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ScalingPoint(scalingPoint)

Parameters:scalingPoint (NXOpen.Point) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

StartBlendScaleFactor

ScalingMethodBuilder.StartBlendScaleFactor

Returns or sets the start blend scale factor.

For scaling by Blending Function, the start scale factor will be applied at the starting of the guide curve.

-------------------------------------

Getter Method

Signature StartBlendScaleFactor()

Returns:
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartBlendScaleFactor(startBlendScaleFactor)

Parameters:startBlendScaleFactor (float) –

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

ScalingMethodBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.