ScalingMethodBuilderScalingOptions Enumeration

NXOpen.GeometricUtilities.ScalingMethodBuilder.ScalingOptions is an alias for NXOpen.GeometricUtilities.ScalingMethodBuilderScalingOptions

class NXOpen.GeometricUtilities.ScalingMethodBuilderScalingOptions

Bases: object

This enum represents the scaling method option.

By default, it is set to Constant. Uniform and Lateral scaling options are invalid if only 1 guide is selected.

Enum Members

Enum Member Enum Member Description
Constant
Constant
ByBlendingFunction
Blending Function
ByAnotherCurve
Another Curve
ByAPoint
A Point
ByAreaLaw
Area Law
ByPerimeterLaw
Perimeter Law
Uniform
Uniform, available only if 2 guides are selected
Lateral
Lateral, available only if 2 guides are selected
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.