RegionTrackerExtremityType Enumeration

NXOpen.GeometricUtilities.RegionTracker.ExtremityType is an alias for NXOpen.GeometricUtilities.RegionTrackerExtremityType

class NXOpen.GeometricUtilities.RegionTrackerExtremityType

Bases: object

This enum represents the type of edge extremity.

This is used to track vertices.

Enum Members

Enum Member Enum Member Description
Start
start
End
end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.