ConicCrossSectionOffsetMethod Enumeration

NXOpen.GeometricUtilities.ConicCrossSection.OffsetMethod is an alias for NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod

class NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod

Bases: object

This enum represents the offset options

Enum Members

Enum Member Enum Member Description
Constant
Constant
Law
Control by law
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.