BooleanOperation Class¶
-
class
NXOpen.GeometricUtilities.
BooleanOperation
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a boolean operation .
New in version NX3.0.1.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Type | Returns or sets the boolean operation type |
Methods¶
Method | Description |
---|---|
GetBooleanOperationAndBody | Get the Boolean operation type and target body |
GetTargetBodies | Get the target bodies @return target bodies of boolean |
SetBooleanOperationAndBody | Set the Boolean operation type and target body |
SetTargetBodies | Set the target bodies |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BooleanOperationBooleanType Enumeration | Boolean operation type. |
Property Detail¶
Type¶
-
BooleanOperation.
Type
¶ Returns or sets the boolean operation type
-------------------------------------
Getter Method
Signature
Type()
Returns: boolean type Return type: NXOpen.GeometricUtilities.BooleanOperationBooleanType
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.GeometricUtilities.BooleanOperationBooleanType
) – boolean typeNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetBooleanOperationAndBody¶
-
BooleanOperation.
GetBooleanOperationAndBody
¶ Get the Boolean operation type and target body
Signature
GetBooleanOperationAndBody()
Returns: a tuple Return type: A tuple consisting of (type, targetBody). type is a NXOpen.GeometricUtilities.BooleanOperationBooleanType
. boolean type targetBody is aNXOpen.Body
. target bodyNew in version NX3.0.1.
Deprecated since version NX4.0.0: Use
GeometricUtilities.BooleanOperation.Type()
andGeometricUtilities.BooleanOperation.GetTargetBodies()
instead.License requirements: None.
GetTargetBodies¶
-
BooleanOperation.
GetTargetBodies
¶ Get the target bodies
Signature
GetTargetBodies()
Returns: target bodies of boolean Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: None.
SetBooleanOperationAndBody¶
-
BooleanOperation.
SetBooleanOperationAndBody
¶ Set the Boolean operation type and target body
Signature
SetBooleanOperationAndBody(type, targetBody)
Parameters: - type (
NXOpen.GeometricUtilities.BooleanOperationBooleanType
) – boolean type - targetBody (
NXOpen.Body
) – target body
New in version NX3.0.1.
Deprecated since version NX4.0.0: Use
GeometricUtilities.BooleanOperation.Type()
andGeometricUtilities.BooleanOperation.SetTargetBodies()
instead.License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
- type (
SetTargetBodies¶
-
BooleanOperation.
SetTargetBodies
¶ Set the target bodies
Signature
SetTargetBodies(targetBodies)
Parameters: targetBodies (list of NXOpen.Body
) – target bodies of booleanNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
BooleanOperation.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.