ParentEquivalencyMapType Enumeration

NXOpen.GeometricUtilities.ParentEquivalencyMap.Type is an alias for NXOpen.GeometricUtilities.ParentEquivalencyMapType

class NXOpen.GeometricUtilities.ParentEquivalencyMapType

Bases: object

enum for map type

Enum Members

Enum Member Enum Member Description
Undefined
undefined
UserDefined
user defined or manual
NameBased
mapped by name
Geometric
mapped by geometric comparison
Inferred
inferred from accepted
Internal
internal ID reuse
Inherited
inherited from other part or operation
Mixed
combination of multiple methods
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.