SaveConstraintsBuilder Class

class NXOpen.GeometricUtilities.SaveConstraintsBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a builder for a Save Constraints.

SaveConstraintsBuilder is not supported in KF.

New in version NX7.0.0.

Properties

Property Description
SaveConstraints Returns or sets the flag indicating whether to save the constraints or not
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

SaveConstraints

SaveConstraintsBuilder.SaveConstraints

Returns or sets the flag indicating whether to save the constraints or not

-------------------------------------

Getter Method

Signature SaveConstraints()

Returns:Flag indicating whether to save the constraints
Return type:bool

New in version NX7.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SaveConstraints(isSaveConstraints)

Parameters:isSaveConstraints (bool) – Flag indicating whether to save the constraints

New in version NX7.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

SaveConstraintsBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.