TriangularFrameBuilder Class¶
-
class
NXOpen.GeometricUtilities.
TriangularFrameBuilder
¶ Bases:
NXOpen.GeometricUtilities.ShapeFrameBuilder
Represents a
NXOpen.GeometricUtilities.TriangularFrameBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Anchor | Returns the anchor of the frame |
AnchorAttachment | Returns or sets the anchor attachment |
NumberVertices | Returns the number of vertices of the frame |
Subtype | Returns or sets the subtype |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetMidpointCoords | Gets the coordinates of the i-th midpoint of the frame with respect to the plane @return coordinates of midpoint relative with respect to plane |
GetVertexCoords | Gets the coordinates of the i-th vertex of the frame with respect to the plane @return coordinates of vertex relative with respect to plane |
SetMidpointCoords | Sets the coordinates of the i-th midpoint of the frame with respect to the plane |
SetVertexCoords | Sets the coordinates of the i-th vertex of the frame with respect to the plane |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TriangularFrameBuilderSubtypes Enumeration | Represents the triangular frame subtypes |
Property Detail¶
Subtype¶
-
TriangularFrameBuilder.
Subtype
¶ Returns or sets the subtype
-------------------------------------
Getter Method
Signature
Subtype()
Returns: Return type: NXOpen.GeometricUtilities.TriangularFrameBuilderSubtypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Subtype(subtype)
Parameters: subtype ( NXOpen.GeometricUtilities.TriangularFrameBuilderSubtypes
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TriangularFrameBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.