TriangularFrameBuilderSubtypes Enumeration

NXOpen.GeometricUtilities.TriangularFrameBuilder.Subtypes is an alias for NXOpen.GeometricUtilities.TriangularFrameBuilderSubtypes

class NXOpen.GeometricUtilities.TriangularFrameBuilderSubtypes

Bases: object

Represents the triangular frame subtypes

Enum Members

Enum Member Enum Member Description
Arbitrary
Arbitrary triangle
Isosceles
Isosceles triangle
Equilateral
Equilateral triangle
Rightangle
Right angle triangle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.