FacePlaneSelectionBuilder Class

class NXOpen.GeometricUtilities.FacePlaneSelectionBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.FacePlaneSelectionBuilder

New in version NX6.0.0.

Properties

Property Description
IsOk Returns or sets the data OK flag
LimitTopolSwitchFinFlag Returns or sets the limit edge switch fin flag
PlaneHelpPoint Returns or sets the user plane cap help point
SelectEdge Returns the select limit edge
SelectFace Returns the select face
SelectPlane Returns or sets the select plane
Tag Returns the Tag for this object.
TrimObject Returns or sets the trim object
UseFaceCapBlend Returns or sets the use face cap blend flag
UsePlaneCapBlend Returns or sets the use plane cap blend

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

FacePlaneSelectionBuilderTrimObjectType Enumeration Specifies the object type for blend endcap objects.

Property Detail

IsOk

FacePlaneSelectionBuilder.IsOk

Returns or sets the data OK flag

-------------------------------------

Getter Method

Signature IsOk()

Returns:
Return type:bool

New in version NX7.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

-------------------------------------

Setter Method

Signature IsOk(isOk)

Parameters:isOk (bool) –

New in version NX7.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

LimitTopolSwitchFinFlag

FacePlaneSelectionBuilder.LimitTopolSwitchFinFlag

Returns or sets the limit edge switch fin flag

-------------------------------------

Getter Method

Signature LimitTopolSwitchFinFlag()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LimitTopolSwitchFinFlag(switchFlag)

Parameters:switchFlag (bool) –

New in version NX8.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

PlaneHelpPoint

FacePlaneSelectionBuilder.PlaneHelpPoint

Returns or sets the user plane cap help point

-------------------------------------

Getter Method

Signature PlaneHelpPoint()

Returns:
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PlaneHelpPoint(helpPoint)

Parameters:helpPoint (NXOpen.Point) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

SelectEdge

FacePlaneSelectionBuilder.SelectEdge

Returns the select limit edge

-------------------------------------

Getter Method

Signature SelectEdge()

Returns:
Return type:NXOpen.ScCollector

New in version NX8.0.0.

License requirements: None.

SelectFace

FacePlaneSelectionBuilder.SelectFace

Returns the select face

-------------------------------------

Getter Method

Signature SelectFace()

Returns:
Return type:NXOpen.GeometricUtilities.FaceSetData

New in version NX6.0.0.

License requirements: None.

SelectPlane

FacePlaneSelectionBuilder.SelectPlane

Returns or sets the select plane

-------------------------------------

Getter Method

Signature SelectPlane()

Returns:
Return type:NXOpen.Plane

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SelectPlane(selectPlane)

Parameters:selectPlane (NXOpen.Plane) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

TrimObject

FacePlaneSelectionBuilder.TrimObject

Returns or sets the trim object

-------------------------------------

Getter Method

Signature TrimObject()

Returns:
Return type:NXOpen.GeometricUtilities.FacePlaneSelectionBuilderTrimObjectType

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature TrimObject(trimObject)

Parameters:trimObject (NXOpen.GeometricUtilities.FacePlaneSelectionBuilderTrimObjectType) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

UseFaceCapBlend

FacePlaneSelectionBuilder.UseFaceCapBlend

Returns or sets the use face cap blend flag

-------------------------------------

Getter Method

Signature UseFaceCapBlend()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseFaceCapBlend(useFaceCapBlend)

Parameters:useFaceCapBlend (bool) –

New in version NX8.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

UsePlaneCapBlend

FacePlaneSelectionBuilder.UsePlaneCapBlend

Returns or sets the use plane cap blend

-------------------------------------

Getter Method

Signature UsePlaneCapBlend()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UsePlaneCapBlend(usePlaneCapBlend)

Parameters:usePlaneCapBlend (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

FacePlaneSelectionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.