FtmFixedCurvesBuilderFixedCurvesContinuityType Enumeration¶
NXOpen.GeometricUtilities.FtmFixedCurvesBuilder.FixedCurvesContinuityType is an alias for NXOpen.GeometricUtilities.FtmFixedCurvesBuilderFixedCurvesContinuityType
-
class
NXOpen.GeometricUtilities.
FtmFixedCurvesBuilderFixedCurvesContinuityType
¶ Bases:
object
Fixed curves continuity type
Enum Members
Enum Member Enum Member Description G0 G0 positionG1 G1 TangentG2 G2 Curvature-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-