RebuildRebuildTypes Enumeration¶
NXOpen.GeometricUtilities.Rebuild.RebuildTypes is an alias for NXOpen.GeometricUtilities.RebuildRebuildTypes
-
class
NXOpen.GeometricUtilities.
RebuildRebuildTypes
¶ Bases:
object
This enum represents the Rebuild type.
Enum Members
Enum Member Enum Member Description NotSet No degree entry or simple integer/enumerable value used to specify the rebuild degree.Manual Specify the rebuild degree manually.Advanced Specify the maximum degree and maximum segments to rebuild.KeepParameterization Keep the parameterization-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-