SpiralPatternOrientType Enumeration

NXOpen.GeometricUtilities.SpiralPattern.OrientType is an alias for NXOpen.GeometricUtilities.SpiralPatternOrientType

class NXOpen.GeometricUtilities.SpiralPatternOrientType

Bases: object

This defines spiral direction method

Enum Members

Enum Member Enum Member Description
Lefthand
Left hand orientation.
Righthand
Right hand orientation.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.