ModlMotionOptions Enumeration¶
NXOpen.GeometricUtilities.ModlMotion.Options is an alias for NXOpen.GeometricUtilities.ModlMotionOptions
-
class
NXOpen.GeometricUtilities.
ModlMotionOptions
¶ Bases:
object
Represents the options of Motion.
Enum Members
Enum Member Enum Member Description AlongCurveAngle Move by AlongCurve-AngleDistanceAngle Move by Distance-AngleDistance Move by DistanceAngle Move by AngleDistanceBetweenPoints Move by Distance between PointsRadialDistance Move by Radial DistancePointToPoint Move by Point to PointRotateByThreePoints Move by Rotate by Three PointsAlignAxisVector Move by Align Axis to VectorCsysToCsys Move by CSYS to CSYSDynamic Move by DynamicDeltaXyz Move by delta XYZNotSet No move-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-