RebuildDegreeTypes Enumeration¶
NXOpen.GeometricUtilities.Rebuild.DegreeTypes is an alias for NXOpen.GeometricUtilities.RebuildDegreeTypes
-
class
NXOpen.GeometricUtilities.
RebuildDegreeTypes
¶ Bases:
object
This enum represents the degree type when the Rebuild option menu is set to None.
Enum Members
Enum Member Enum Member Description Cubic The rebuild degree is cubic.Quintic The rebuild degree is quintic-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-