PatternIncrementsList Class

class NXOpen.GeometricUtilities.PatternIncrementsList

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

list of NXOpen.GeometricUtilities.PatternIncrementItem objects.

New in version NX7.5.0.

Properties

Property Description
List Returns the list of NXOpen.GeometricUtilities.PatternIncrementItem objects.
Tag Returns the Tag for this object.

Methods

Method Description
CreatePatternIncrementItem This is the default creator for NXOpen.GeometricUtilities.PatternIncrementItem.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

List

PatternIncrementsList.List

Returns the list of NXOpen.GeometricUtilities.PatternIncrementItem objects.

-------------------------------------

Getter Method

Signature List()

Returns:
Return type:NXOpen.GeometricUtilities.PatternIncrementItemList

New in version NX7.5.0.

License requirements: None.

Method Detail

CreatePatternIncrementItem

PatternIncrementsList.CreatePatternIncrementItem

Overloaded method CreatePatternIncrementItem

  • CreatePatternIncrementItem()
  • CreatePatternIncrementItem(masterExpression)

-------------------------------------

This is the default creator for NXOpen.GeometricUtilities.PatternIncrementItem. Caution: This should never be called!

Signature CreatePatternIncrementItem()

Returns:
Return type:NXOpen.GeometricUtilities.PatternIncrementItem

New in version NX7.5.0.

License requirements: None.

-------------------------------------

This is the actual creator for NXOpen.GeometricUtilities.PatternIncrementItem.

Signature CreatePatternIncrementItem(masterExpression)

Parameters:masterExpression (NXOpen.Expression) – the master expression
Returns:
Return type:NXOpen.GeometricUtilities.PatternIncrementItem

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Validate

PatternIncrementsList.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.