BridgeCurveConnectivityFaceDirectionOptions Enumeration¶
NXOpen.GeometricUtilities.BridgeCurveConnectivity.FaceDirectionOptions is an alias for NXOpen.GeometricUtilities.BridgeCurveConnectivityFaceDirectionOptions
-
class
NXOpen.GeometricUtilities.
BridgeCurveConnectivityFaceDirectionOptions
¶ Bases:
object
Tangent constraint direction when end is attached to a face
Enum Members
Enum Member Enum Member Description Sectional Sectional directionIsoU Along U iso-parameterIsoV Along V iso-parameter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-