OnPathDistancePatternSpacing Class

class NXOpen.GeometricUtilities.OnPathDistancePatternSpacing

Bases: NXOpen.GeometricUtilities.PatternSpacing

defines the various ways pattern instances can be spaced within the pattern, particularly in the context of the PatternDefinition class.

New in version NX7.5.0.

Properties

Property Description
NCopies Returns the number of copies the pattern will generated in this direction
OnPathPitchDistance Returns the distance for the spacing of the pattern from one instance to the next.
OnPathSpanDistance Returns the distance for the spacing of the pattern for the entire pattern.
SpaceType Returns or sets the type of spacing to be used by the pattern
SpacingsList Returns the list of spacings (Expression or OnPathDimBuilder) to be used in this direction
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

OnPathPitchDistance

OnPathDistancePatternSpacing.OnPathPitchDistance

Returns the distance for the spacing of the pattern from one instance to the next.

-------------------------------------

Getter Method

Signature OnPathPitchDistance()

Returns:
Return type:NXOpen.GeometricUtilities.OnPathDimensionBuilder

New in version NX7.5.0.

License requirements: None.

OnPathSpanDistance

OnPathDistancePatternSpacing.OnPathSpanDistance

Returns the distance for the spacing of the pattern for the entire pattern.

-------------------------------------

Getter Method

Signature OnPathSpanDistance()

Returns:
Return type:NXOpen.GeometricUtilities.OnPathDimensionBuilder

New in version NX7.5.0.

License requirements: None.

Method Detail

Validate

OnPathDistancePatternSpacing.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.