CurveFitDataMethod Enumeration

NXOpen.GeometricUtilities.CurveFitData.Method is an alias for NXOpen.GeometricUtilities.CurveFitDataMethod

class NXOpen.GeometricUtilities.CurveFitDataMethod

Bases: object

Represents the curve fitting method in the case of advanced fitting

Enum Members

Enum Member Enum Member Description
DegreeAndSegments
Degree and Segments
DegreeAndTolerance
Degree and Tolerance
KeepParameterization
Keep Parameterization
AutoFit
Auto Fit
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.