CurveFitOptionsFitMethod Enumeration

NXOpen.GeometricUtilities.CurveFitOptions.FitMethod is an alias for NXOpen.GeometricUtilities.CurveFitOptionsFitMethod

class NXOpen.GeometricUtilities.CurveFitOptionsFitMethod

Bases: object

Represents the curve fit method

Enum Members

Enum Member Enum Member Description
Cubic
Cubic
Quintic
Quintic
Advanced
Advanced
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.