DepthSkewBuilder Class

class NXOpen.GeometricUtilities.DepthSkewBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

This class provides ability to specify a depth and a skew value.

New in version NX6.0.0.

Properties

Property Description
Depth Returns the depth
Skew Returns the skew
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Depth

DepthSkewBuilder.Depth

Returns the depth

-------------------------------------

Getter Method

Signature Depth()

Returns:
Return type:NXOpen.Expression

New in version NX6.0.0.

License requirements: None.

Skew

DepthSkewBuilder.Skew

Returns the skew

-------------------------------------

Getter Method

Signature Skew()

Returns:
Return type:NXOpen.Expression

New in version NX6.0.0.

License requirements: None.

Method Detail

Validate

DepthSkewBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.