ProjectionOptionsDirectionType Enumeration

NXOpen.GeometricUtilities.ProjectionOptions.DirectionType is an alias for NXOpen.GeometricUtilities.ProjectionOptionsDirectionType

class NXOpen.GeometricUtilities.ProjectionOptionsDirectionType

Bases: object

This enum represents the projection direction types

Enum Members

Enum Member Enum Member Description
FaceNormal
Face Normal
CrvPlaneNormal
Curve plane Normal
Vector
Vector Constructor
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.