CurveSettings Class¶
-
class
NXOpen.GeometricUtilities.
CurveSettings
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the curve settings data
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CurveFitData | Returns the curve fit data |
InputCurvesOption | Returns the input curves option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveFitData¶
-
CurveSettings.
CurveFitData
¶ Returns the curve fit data
-------------------------------------
Getter Method
Signature
CurveFitData()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitData
New in version NX11.0.0.
License requirements: None.
InputCurvesOption¶
-
CurveSettings.
InputCurvesOption
¶ Returns the input curves option
-------------------------------------
Getter Method
Signature
InputCurvesOption()
Returns: Return type: NXOpen.GeometricUtilities.CurveOptions
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CurveSettings.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.