RefitControlBuilderRefitControlMethod Enumeration

NXOpen.GeometricUtilities.RefitControlBuilder.RefitControlMethod is an alias for NXOpen.GeometricUtilities.RefitControlBuilderRefitControlMethod

class NXOpen.GeometricUtilities.RefitControlBuilderRefitControlMethod

Bases: object

Refit method

Enum Members

Enum Member Enum Member Description
KeepParameterization
Keep parameterization
DegreePatches
Degree and patches
DegreeTolerance
Degree and tolerance
PatchTolerance
Patch and tolerance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.