RadiusMethod Enumeration

class NXOpen.GeometricUtilities.RadiusMethod

Bases: object

This enum represents the radius options Enum Members

Enum Member Enum Member Description
Constant
Constant
Law
Control by law
Tangency
Control by tangency
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.