OrientationMethodBuilderOrientationOptions Enumeration¶
NXOpen.GeometricUtilities.OrientationMethodBuilder.OrientationOptions is an alias for NXOpen.GeometricUtilities.OrientationMethodBuilderOrientationOptions
-
class
NXOpen.GeometricUtilities.
OrientationMethodBuilderOrientationOptions
¶ Bases:
object
This enum represents the orientation option.
By default, it is set to Fixed. Angular Law orientation option is invalid if 2 guides are selected.
Enum Members
Enum Member Enum Member Description Fixed FixedByFaceNormals Face NormalsByVectorDirection Vector DirectionByAnotherCurve Another CurveByAPoint A PointByAngularLaw Angular LawByForcedDirection Forced Direction-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-