EnumTestAnimals Enumeration

NXOpen.GeometricUtilities.EnumTest.Animals is an alias for NXOpen.GeometricUtilities.EnumTestAnimals

class NXOpen.GeometricUtilities.EnumTestAnimals

Bases: object

Animals are healthy and taste good

Enum Members

Enum Member Enum Member Description
Pika
rabbit with mouse ears
Aardvark
no better animal name
Hippo
Hippos are big
Snake
Snakes are not really slimey
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.