ConicCrossSection Class¶
-
class
NXOpen.GeometricUtilities.
ConicCrossSection
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a conic section data for face blend.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ConicMethod | Returns or sets the conic method for the advanced symmetric conic section with face blend |
Depth | Returns the depth expression for the conic section with face blend |
DepthLawControl | Returns the Depth Law builder |
DepthOption | Returns or sets the depth option for the conic section with face blend |
FirstConstraintCurveCollector | Returns or sets the first constraint curve collector |
FirstLawControl | Returns the First Offset Law builder |
FirstOffset | Returns the first offset for the conic section with face blend |
FirstOffsetOption | Returns or sets the first offset option for the conic section with face blend |
OffsetSkewRatio | Returns the offset skew ratio expression for the conic section with face blend |
Rho | Returns the rho expression for the conic section with face blend |
RhoLawControl | Returns the Rho Law builder |
RhoOption | Returns or sets the rho option for the conic section with face blend |
SecondConstraintCurveCollector | Returns or sets the second constraint curve collector |
SecondLawControl | Returns the Second Offset Law builder |
SecondOffset | Returns the second offset for the conic section with face blend |
SecondOffsetOption | Returns or sets the second offset option for the conic section with face blend |
ShapeSkew | Returns the shape skew expression for the conic section with face blend |
ShapeSkewLawControl | Returns the Shape Skew Law builder |
ShapeSkewOption | Returns or sets the shape skew option for the conic section with face blend |
Tag | Returns the Tag for this object. |
TransitionLinkFlag | Returns or sets the flag to link multi-transition law types |
Methods¶
Method | Description |
---|---|
SetFirstOffset | Sets the first offset for the conic section with face blend. |
SetLawControlConstantDepth | Sets a constant radius for the depth law control of the conic section with face blend. |
SetLawControlConstantFirstOffset | Sets a constant radius for the first law control of the conic section with face blend. |
SetLawControlConstantRho | Sets a constant radius for the rho law control of the conic section with face blend. |
SetLawControlConstantSecondOffset | Sets a constant radius for the second law control of the conic section with face blend. |
SetLawControlConstantShapeSkew | Sets a constant radius for the shape skew law control of the conic section with face blend. |
SetLawControlDepthEndRadius | Sets a end radius for the depth law control of the conic section with face blend. |
SetLawControlDepthStartRadius | Sets a start radius for the depth law control of the conic section with face blend. |
SetLawControlFirstOffsetEndRadius | Sets a end radius for the first law control of the conic section with face blend. |
SetLawControlFirstOffsetStartRadius | Sets a start radius for the first law control of the conic section with face blend. |
SetLawControlRhoEndRadius | Sets a end radius for the rho law control of the conic section with face blend. |
SetLawControlRhoStartRadius | Sets a start radius for the rho law control of the conic section with face blend. |
SetLawControlSecondOffsetEndRadius | Sets a end radius for the second law control of the conic section with face blend. |
SetLawControlSecondOffsetStartRadius | Sets a start radius for the second law control of the conic section with face blend. |
SetLawControlShapeSkewEndRadius | Sets a end radius for the shape skew law control of the conic section with face blend. |
SetLawControlShapeSkewStartRadius | Sets a start radius for the shape skew law control of the conic section with face blend. |
SetRho | Sets a rho expression for the conic section with face blend. |
SetSecondOffset | Sets the second offset for the conic section with face blend. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConicCrossSectionDefineMethod Enumeration | This enum represents the conic method for advanced symmetric conic |
ConicCrossSectionDepthMethod Enumeration | This enum represents the depth option |
ConicCrossSectionOffsetMethod Enumeration | This enum represents the offset options |
ConicCrossSectionRhoMethod Enumeration | This enum represents the rho options |
ConicCrossSectionShapeSkewMethod Enumeration | This enum represents the shape skew option |
Property Detail¶
ConicMethod¶
-
ConicCrossSection.
ConicMethod
¶ Returns or sets the conic method for the advanced symmetric conic section with face blend
-------------------------------------
Getter Method
Signature
ConicMethod()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionDefineMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicMethod(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionDefineMethod
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Depth¶
-
ConicCrossSection.
Depth
¶ Returns the depth expression for the conic section with face blend
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
DepthLawControl¶
-
ConicCrossSection.
DepthLawControl
¶ Returns the Depth Law builder
-------------------------------------
Getter Method
Signature
DepthLawControl()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX10.0.0.
License requirements: None.
DepthOption¶
-
ConicCrossSection.
DepthOption
¶ Returns or sets the depth option for the conic section with face blend
-------------------------------------
Getter Method
Signature
DepthOption()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionDepthMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthOption(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionDepthMethod
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstConstraintCurveCollector¶
-
ConicCrossSection.
FirstConstraintCurveCollector
¶ Returns or sets the first constraint curve collector
-------------------------------------
Getter Method
Signature
FirstConstraintCurveCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstConstraintCurveCollector(collector)
Parameters: collector ( NXOpen.ScCollector
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FirstLawControl¶
-
ConicCrossSection.
FirstLawControl
¶ Returns the First Offset Law builder
-------------------------------------
Getter Method
Signature
FirstLawControl()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX5.0.0.
License requirements: None.
FirstOffset¶
-
ConicCrossSection.
FirstOffset
¶ Returns the first offset for the conic section with face blend
-------------------------------------
Getter Method
Signature
FirstOffset()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
FirstOffsetOption¶
-
ConicCrossSection.
FirstOffsetOption
¶ Returns or sets the first offset option for the conic section with face blend
-------------------------------------
Getter Method
Signature
FirstOffsetOption()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstOffsetOption(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OffsetSkewRatio¶
-
ConicCrossSection.
OffsetSkewRatio
¶ Returns the offset skew ratio expression for the conic section with face blend
-------------------------------------
Getter Method
Signature
OffsetSkewRatio()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Rho¶
-
ConicCrossSection.
Rho
¶ Returns the rho expression for the conic section with face blend
-------------------------------------
Getter Method
Signature
Rho()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
RhoLawControl¶
-
ConicCrossSection.
RhoLawControl
¶ Returns the Rho Law builder
-------------------------------------
Getter Method
Signature
RhoLawControl()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX5.0.0.
License requirements: None.
RhoOption¶
-
ConicCrossSection.
RhoOption
¶ Returns or sets the rho option for the conic section with face blend
-------------------------------------
Getter Method
Signature
RhoOption()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionRhoMethod
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RhoOption(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionRhoMethod
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondConstraintCurveCollector¶
-
ConicCrossSection.
SecondConstraintCurveCollector
¶ Returns or sets the second constraint curve collector
-------------------------------------
Getter Method
Signature
SecondConstraintCurveCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondConstraintCurveCollector(collector)
Parameters: collector ( NXOpen.ScCollector
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SecondLawControl¶
-
ConicCrossSection.
SecondLawControl
¶ Returns the Second Offset Law builder
-------------------------------------
Getter Method
Signature
SecondLawControl()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX5.0.0.
License requirements: None.
SecondOffset¶
-
ConicCrossSection.
SecondOffset
¶ Returns the second offset for the conic section with face blend
-------------------------------------
Getter Method
Signature
SecondOffset()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
SecondOffsetOption¶
-
ConicCrossSection.
SecondOffsetOption
¶ Returns or sets the second offset option for the conic section with face blend
-------------------------------------
Getter Method
Signature
SecondOffsetOption()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondOffsetOption(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionOffsetMethod
) –New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ShapeSkew¶
-
ConicCrossSection.
ShapeSkew
¶ Returns the shape skew expression for the conic section with face blend
-------------------------------------
Getter Method
Signature
ShapeSkew()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ShapeSkewLawControl¶
-
ConicCrossSection.
ShapeSkewLawControl
¶ Returns the Shape Skew Law builder
-------------------------------------
Getter Method
Signature
ShapeSkewLawControl()
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX10.0.0.
License requirements: None.
ShapeSkewOption¶
-
ConicCrossSection.
ShapeSkewOption
¶ Returns or sets the shape skew option for the conic section with face blend
-------------------------------------
Getter Method
Signature
ShapeSkewOption()
Returns: Return type: NXOpen.GeometricUtilities.ConicCrossSectionShapeSkewMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeSkewOption(method)
Parameters: method ( NXOpen.GeometricUtilities.ConicCrossSectionShapeSkewMethod
) –New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TransitionLinkFlag¶
-
ConicCrossSection.
TransitionLinkFlag
¶ Returns or sets the flag to link multi-transition law types
-------------------------------------
Getter Method
Signature
TransitionLinkFlag()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionLinkFlag(transitionLinkFlag)
Parameters: transitionLinkFlag (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
SetFirstOffset¶
-
ConicCrossSection.
SetFirstOffset
¶ Sets the first offset for the conic section with face blend.
Signature
SetFirstOffset(offset)
Parameters: offset (str) – New in version NX4.0.0.
Deprecated since version NX9.0.0: To set the value of the expression modify the expression directly using
NXOpen.GeometricUtilities.ConicCrossSection.FirstOffset()
andNXOpen.Expression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlConstantDepth¶
-
ConicCrossSection.
SetLawControlConstantDepth
¶ Sets a constant radius for the depth law control of the conic section with face blend.
Signature
SetLawControlConstantDepth(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlConstantFirstOffset¶
-
ConicCrossSection.
SetLawControlConstantFirstOffset
¶ Sets a constant radius for the first law control of the conic section with face blend.
Signature
SetLawControlConstantFirstOffset(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlConstantRho¶
-
ConicCrossSection.
SetLawControlConstantRho
¶ Sets a constant radius for the rho law control of the conic section with face blend.
Signature
SetLawControlConstantRho(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlConstantSecondOffset¶
-
ConicCrossSection.
SetLawControlConstantSecondOffset
¶ Sets a constant radius for the second law control of the conic section with face blend.
Signature
SetLawControlConstantSecondOffset(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlConstantShapeSkew¶
-
ConicCrossSection.
SetLawControlConstantShapeSkew
¶ Sets a constant radius for the shape skew law control of the conic section with face blend.
Signature
SetLawControlConstantShapeSkew(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlDepthEndRadius¶
-
ConicCrossSection.
SetLawControlDepthEndRadius
¶ Sets a end radius for the depth law control of the conic section with face blend.
Signature
SetLawControlDepthEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlDepthStartRadius¶
-
ConicCrossSection.
SetLawControlDepthStartRadius
¶ Sets a start radius for the depth law control of the conic section with face blend.
Signature
SetLawControlDepthStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlFirstOffsetEndRadius¶
-
ConicCrossSection.
SetLawControlFirstOffsetEndRadius
¶ Sets a end radius for the first law control of the conic section with face blend.
Signature
SetLawControlFirstOffsetEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlFirstOffsetStartRadius¶
-
ConicCrossSection.
SetLawControlFirstOffsetStartRadius
¶ Sets a start radius for the first law control of the conic section with face blend.
Signature
SetLawControlFirstOffsetStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlRhoEndRadius¶
-
ConicCrossSection.
SetLawControlRhoEndRadius
¶ Sets a end radius for the rho law control of the conic section with face blend.
Signature
SetLawControlRhoEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlRhoStartRadius¶
-
ConicCrossSection.
SetLawControlRhoStartRadius
¶ Sets a start radius for the rho law control of the conic section with face blend.
Signature
SetLawControlRhoStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlSecondOffsetEndRadius¶
-
ConicCrossSection.
SetLawControlSecondOffsetEndRadius
¶ Sets a end radius for the second law control of the conic section with face blend.
Signature
SetLawControlSecondOffsetEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlSecondOffsetStartRadius¶
-
ConicCrossSection.
SetLawControlSecondOffsetStartRadius
¶ Sets a start radius for the second law control of the conic section with face blend.
Signature
SetLawControlSecondOffsetStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlShapeSkewEndRadius¶
-
ConicCrossSection.
SetLawControlShapeSkewEndRadius
¶ Sets a end radius for the shape skew law control of the conic section with face blend.
Signature
SetLawControlShapeSkewEndRadius(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetLawControlShapeSkewStartRadius¶
-
ConicCrossSection.
SetLawControlShapeSkewStartRadius
¶ Sets a start radius for the shape skew law control of the conic section with face blend.
Signature
SetLawControlShapeSkewStartRadius(radius)
Parameters: radius (str) – The value to be set New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetRho¶
-
ConicCrossSection.
SetRho
¶ Sets a rho expression for the conic section with face blend.
Signature
SetRho(rho)
Parameters: rho (str) – New in version NX4.0.0.
Deprecated since version NX9.0.0: To set the value of the expression modify the expression directly using
NXOpen.GeometricUtilities.ConicCrossSection.Rho()
andNXOpen.Expression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
SetSecondOffset¶
-
ConicCrossSection.
SetSecondOffset
¶ Sets the second offset for the conic section with face blend.
Signature
SetSecondOffset(offset)
Parameters: offset (str) – New in version NX4.0.0.
Deprecated since version NX9.0.0: To set the value of the expression modify the expression directly using
NXOpen.GeometricUtilities.ConicCrossSection.SecondOffset()
andNXOpen.Expression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
ConicCrossSection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.