ConicCrossSectionDefineMethod Enumeration

NXOpen.GeometricUtilities.ConicCrossSection.DefineMethod is an alias for NXOpen.GeometricUtilities.ConicCrossSectionDefineMethod

class NXOpen.GeometricUtilities.ConicCrossSectionDefineMethod

Bases: object

This enum represents the conic method for advanced symmetric conic

Enum Members

Enum Member Enum Member Description
BoundaryPlusCenter
conic shape controlled by boundary and center values
BoundaryPlusRho
conic shape controlled by boundary and rho values
CenterPlusRho
conic shape controlled by center and rho values
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.