SpinePointDataParameterType Enumeration

NXOpen.GeometricUtilities.SpinePointData.ParameterType is an alias for NXOpen.GeometricUtilities.SpinePointDataParameterType

class NXOpen.GeometricUtilities.SpinePointDataParameterType

Bases: object

Parameter type

Enum Members

Enum Member Enum Member Description
Normal
Percent
Parameter expressed as percent arc length
Length
Parameter expressed as arc length
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.