ContinuityContinuityTypes Enumeration

NXOpen.GeometricUtilities.Continuity.ContinuityTypes is an alias for NXOpen.GeometricUtilities.ContinuityContinuityTypes

class NXOpen.GeometricUtilities.ContinuityContinuityTypes

Bases: object

Continuity type.

Enum Members

Enum Member Enum Member Description
G0
G0 continuity
G1
G1 continuity
G2
G2 continuity
G3
G3 continuity
Free
Free continuity
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.