OrientXpressTestBuilderAxisBlock Enumeration

NXOpen.GeometricUtilities.OrientXpressTestBuilder.AxisBlock is an alias for NXOpen.GeometricUtilities.OrientXpressTestBuilderAxisBlock

class NXOpen.GeometricUtilities.OrientXpressTestBuilderAxisBlock

Bases: object

the options to show or hide the axis block

Enum Members

Enum Member Enum Member Description
Show
Test show axis block
Hide
Test hide axis block
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.